news 1 week ago

These 3 Eco-Friendly Products Get Us One Step Closer to Saving the Planet

StackCommerce — shannon

In case you haven’t noticed, our planet’s resources are dwindling and it’s up to us to slow things down before it’s too late. And while sometimes it can feel overwhelming when it comes to finding ways to cut back and conserve, there are little things you can do in your daily life that actually make a world of difference.

We’ve found three fantastic products that you can incorporate into your eco-friendly household, making the world a safer, cleaner place for everyone. And the best part? It won’t cost you much at all. 

1. pH Restore Alkaline Water Filter Pitcher

Look, you prefer filtered water to tap water so sometimes buying bottled water is the only option, right? Well, there are plenty of ways to enjoy clean, filtered water without buying plastic bottles that pollute the earth. Meet the pH Restore Alkaline Water Filter Pitcher, a hand-held system that removes chemicals, adding beneficial minerals like selenium and calcium as it filters. When you pour water into the pitcher, it increases its alkalinity (pH level) and eliminates free radicals thanks to its high negative Oxidization Reduction Potential (ORP). While you can’t actually see all the action taking place with the naked eye, you’ll taste and smell the difference of this clean, fresh drinking water. 

This slight water adjustment can do wonders for your everyday health, keeping you well hydrated and giving you more energy and mental clarity. That’s because removing the heavy chemicals that are often found in tap water, like lead, zinc, and copper, completely change the water’s formation, turning into micro-clusters that can be absorbed more easily into your cells and to the rest of your body. You’ve never tasted water quite like this. 

The deal: The pH Restore Alkaline Water Filter Pitcher can be yours for $39.99 down from $89 bucks.

2. The Aquamiser Water Saving Atomizer: 4-Pack

Have you ever stopped to think about how much water you waste in a day? According to US BPA, the average family wastes up to a whopping 180 gallons per week! But sometimes it’s hard to control since our faucets and showerheads often streamline way more water than we actually need. That’s where the Aquamiser Water Saving Atomizer comes into play. This ingeniously engineered automizer can save 95% more water whenever you use it! 

The little adapter fits on just about any faucet head and takes just seconds to install. When you use it, you’ll have two different modes to choose from that can easily be activated with a single “twist” of the nozzle. Once it’s attached, you’ll notice water in a “misting” form, rather than its regular, heavier flow. While it may not seem like it’s giving you enough water to say, wash your hands, you’ll notice that it actually gives you just the right amount of liquid.  Just by using this chrome-plated, food-grade nozzle, you’ll save 10 times more water than the best water-saving alternatives out there. 

The nozzles also come in packs of four, allowing you to convert every sink in your home or office into a water-conserving one!

The deal: Start conserving with the Aquamiser Water Saving Atomizer: 4-Pack now 46% off at just $31.99.

3. Assorted Silicone Reusable Straws by Softy Straws

These days, many restaurants and grocery stores are stocking up on plastic-free items like bamboo toothbrushes, metal reusable bottles, and of course, straws. But while reusable straws made of alternative materials like bamboo or paper are recyclable, they’re not the most convenient — if you’ve ever taken a sip out of a soggy straw, you understand exactly what we’re talking about. That’s why people everywhere are loving these reusable Softy Straws made of silicone! 

These reusable Softy Straws are a great way for you to cut back on plastic use, whether you’re using them at home or taking them with you on-the-go. The premium 9″ silicone straws are comprised of silicone, making them a safe, easy-to-clean option for both you and your family to use on the daily. And unlike reusable eco-friendly straws made of metal, these Softy Straws won’t become super hot or cold to the touch as you slurp.

The Softy Straw pack includes four, colorful reusable silicone straws along with a convenient cleaning tool.  It’s also worth noting that the straws are extra-long in length, making them ideal for using in tumblers. While using Softy Straws every day may not seem like it has a big impact on the earth, it’s a small thing you can do to contribute to the world’s well-being.

The deal: Snag your discounted Softy Straws Assorted Silicone Reusable Straws for just $17.99.

Like this deal? Check out Vault — you’ll get four premium tools, including NordVPN and Dashlane, to supercharge your online security. Try it free for 14 days now!

All prices subject to change.